This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP55231: LP55231

Part Number: LP55231

I want to use LP55231 to drive 12VDC RGB LED Strip with common anode.

I need circuit design using LP55231 to drive 12VDC RGB LED strip using MOSFET

Can you send reference design for this?

  • Hi Mane,

    Nice to hear you!

    But unfortunately, LP55231 cannot support 12V DC value for the output pins, the value for Voutput is VDD + 0.3 V with 6 V maximum.

    Could you share me more details about your LED strip, like the schematics, so I can find more suitable device for you.

    Thanks!

    BR,

    Ives Li