Dear Sir,
Could you recommend the thermo area of PCB(high K, JESD 51-7) for TL5209DR(SOIC), Vin=6V, Vout=5V@0.5A
Thanks
Jacob
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
Could you recommend the thermo area of PCB(high K, JESD 51-7) for TL5209DR(SOIC), Vin=6V, Vout=5V@0.5A
Thanks
Jacob
Hello Jacob,
Are you asking the junction temperature for the TL5209 using the standard board at that Vin and load or are you asking for specifics about the standard board itself?
Regards,
Ron Michallick
Jacob,
I found this link that has board and trace dimensions. focus.tij.co.jp/jp/lit/an/szza017a/szza017a.pdf
The power disspation is based on quiescent current and output current.
(6V-5V) * 500mA = 500mW
6V * 8mA = 48mW (typical)
Total power 548mW
Tj = Ta + 97C/W * 0.548W or Tj = Ta + 53C
Regards,
Ron Michallick