This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61070: Inductor Selection >10uH

Part Number: TPS61070


Hello,

Working on a design with VIN min = 1.6V, Vout = 3V, and Iout max = 30mA. By my calculations, this would require an inductor greater than the recommended 10uH maximum. Should we use 10uH or is it ok to exceed this and use a 22uH inductor?

Thanks,

Michael