Hi
If the input voltage is equal to or less than the output voltage Is there a pass-through function?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Gareth,
The converter will go into 99% duty cycle when input voltage is less than setpoint output voltage.
The high-side FET will be on 99+% of the time such that VOUT≈VIN.
Hope this helps,
-Orlando
Hi Gareth,
No this device does not have 100% duty cycle capability.
Our maximum duty cycle will be 99-99.9% depending on switching frequency.
Hope this helps,
-Orlando