Hi,
Kindly advise if there is any suitable TI device to limit the current to <200mA. However the input and output voltage is maintained at +/-20V. Browse through TI site and seems like all are below 5.5V for USB application. Another option I've is the LM317 (cheaper) and TPS2590 (very expensive). Kindly do advise is there is alternative.
Thanks.