Other Parts Discussed in Thread: TLV767-Q1, , TPS7B86-Q1
Hi team,
Customer is choosing LDO for transmission control unit and has high ambient temperature VIN=14V,VOUT=5V,Iout=150mA;(Ta=115℃);
I'm promoting TLV766-Q1 but customer think the thermal resistance is too large, when I check TLV767-Q1 I found the thermal information chart is exactly the same. I don't understand why a 1A rating LDO has the same thermal performance with it's p2p 0.5A version? Previously I though larger curretn rating LDO should have smaller thermal resistance. If not, how can it support larger load current?
Thank you
Scarlett