This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1825: Recommendation requests and technical support requests for values of R and C located between EAOUT and INV pins.

Part Number: UC1825


Hello

Thank you for responding to my previous inquiry.

I'm writing to ask you some additional questions.

1. You said that R and C are required between EAOUT and INV pins, Can you recommend the appropriate R and C values for the above circuit?

2. In the above circuit, the output of EAOUT pin is 5V in normal operation and 2V in abnormal operation.(The output is reduced.) I was wondering if the R and C between EAOUT and INV have an effect on the reason why the output decreases.

Thank you for your response.