Hello,
I am working on implementing a boost converter using the TPS61088. May I ask for a bit of help in assessing the SW pin switching characteristics to see if they are within safe limits?
The boost converter has the following parameters:
- Vin = 5V, Vout = 12V, Iout ~1-1.2A resistive load
- SW pin absolute ratings (as per the datasheet): -0.3V to 14.5V (I believe these are DC values), and short time transient AC voltage can be as high as 20V according to the forum.
The SW pin voltages are as follows:
- Spikes on the SW pin of 15.1V for about 10ns. This seems fine given the transient AC voltage rating of the chip
- When low, the SW pin maintains -0.7V. This is a lot more concerning

The measurements were taken using a 50Mhz oscilloscope with local ground connection on the PGND plane.
Please let me know if any additional information such as schematics or layout would be helpful.