This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61094: No Supercapacitor scheme

Part Number: TPS61094


Hi Best Regards

I want to use the TPS61094 in boost mode.

The condition are:

* Always the Vin will be a Li-ion Battery 3.3V-4.2V

* Vout voltage must be 5V.

* The TPS will supply a sensor, maximum current 300mA.

* No need Supercapacitor or backup feature

Could you please double check the schematic ?