This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3852-Q1: technical issue

Part Number: TPS3852-Q1

hi team,

could you help support this problem.

VDD to 3.3V, CWD to ground via 100pF capacitance, SET1=1
If the VDD voltage remains at 3.3V, What should the WDO output waveform state when the WDI input waveform is in the tPULSE > tWDU(min) and tPULSE < tWDL(max) non-normal operating range?