The followings are question for LM25143-Q1 from a customer.
1. データーシートの図9.9のようなインターリーブで 3.3V出力の仕様をWebenchで回路生成させるとVCCXはGND接続となります。
一方、図9.9(DS_P33)でのVCCXはVout(3.3V)に接続されています。この違いは何が原因ですか?
If you generate a simulation bench circuit with Webench for 3.3V output specifications with interleaving as shown in Figure 9.9 of the datasheet, VCCX is connected to GND.
On the other hand, VCCX in Figure 9.9 (Datasheet, Page.33) is connected to Vout (3.3V). What causes this difference?
2. ”VCCX > 4.3V の場合、VCCX は VCC に内部で接続され、内部の VCC レギュレータはディセーブルになります。”とデーターシート(P6)記載あります。前記の質問1.ではVCCXが3.3Vに接続、又はGNDに接続先されたケースですが、いずれもVCCXは4.3V未満です。接続先は異なりますが、どちらのケースもVCCは同じ状態でしょうか?
"When VCCX > 4.3V, VCCX is internally connected to VCC and the internal VCC regulator is disabled." is stated in the datasheet (P6). In the above question 1, VCCX is connected to 3.3V or connected to GND, but in both cases VCCX is less than 4.3V. The connection destination is different, but is VCC in the same state in both cases?
3. インダクタ DCR 電流センシング方式で過電流値の設定は式12(DS_P29)と思われます。
式12が理解できません。 具体的に例えばインターリーブ3.3V 20AでLo=470nH DCr=3.6mΩのケースでご説明頂けると助かります。
式の記述に関する質問もあります。Vcs(s)は電圧ではないのですか?単位はs(秒)となっています。それとも検出時間ですか? また式の中にある”s”も何を指しているのか不明です。(1+s*Lo/Rdcrのところにあるs)
The setting of the overcurrent value in the inductor DCR current sensing method seems to be Equation 12 (DS_P29).
I don't understand equation 12. It would be helpful if you could give a specific example of a case where Lo = 470nH DCr = 3.6mΩ at interleaved 3.3V 20A.
I also have a question about writing expressions. Isn't Vcs(s) a voltage? The unit is s (seconds). Or is it detection time? Also, it is unclear what the "s" in the formula refers to. (1+s*Lo/s at Rdcr)
Best Regards, Taki