Other Parts Discussed in Thread: BQ51003, BQ51013B-Q1, BQ51013B
Hi, we are using a BQ51050B for Qi charging. The problem is that the BQ51050 won't charge the battery if its voltage is below 3V.
This can happen if the battery drains after a long period of non use and the PCM (2.7V) switches off, however this problem also happens with the PCM removed.
Our battery is 100mAh which we would like to charge a 1C.
According to the data sheet if the battery is below Vlowv (approx. 3.0V) it should enter PRECHG mode but it doesn't under any circumstances.
We've tried with different Chargers and Qi antennas, our current charger uses a Renesas P9235A. With the Renesas part we can see normal operation and communications between the devices.
Also, the circuit should have a charge current limit of 100mA with R36 at 2K94 and R40 at 200R but it is about 50mA? If we use a 1K52 for R36 we do get a 100mA charge. This indicates Kilim is well outside spec!?
We have tried removing our attempted fix of D1/R33.
The schematic is attached.
Do you have any idea what could be going wrong?
Thanks Ian