1、The schematic diagram is shown in the following figure, VBUS=0, Vbat=7.6V

2、 SDRV_ CTRL default value 00。The waveform of VSYS unloaded SDRV is shown in Figure 1, and the voltage of VSYS is normal. VSYS is connected to a 50mA constant current source, and the SDRV waveform is shown in Figure 2. VSYS has been continuously on and off. The waveform of the SDRV connected to the adapter is shown in Figure 3, and the voltage of the VSYS is normal.




3、In the second test, without the adapter, the ship mos cannot function properly. How can I enter ship mode or shutdown mode。
3、