Part Number: TPS23754
Other Parts Discussed in Thread: PMP6812,
Hello, Team
I have implemented a power circuit using TPS23754. The input power is solely from a 54V adapter, and the circuit demands an output of 12V 2.5A.
The issue I am facing is that although the output voltage is 12V, when the power reaches around 5W(54V,0.09A), the FET(U20) starts to heat up significantly, reaching temperatures as high as 100 degrees Celsius. The VC measures 18V, while the GATE receives 12V. VB shows a reading of 5.1V.
I have attempted to modify the APD and PPD pins by attenuating the input voltage through resistors, but the problem persists, and I haven't found a solution.
I would appreciate your assistance in troubleshooting this issue.