I've designed the LMR64010XMFX/NOPB into a circuit to convert 12V to 24V. I've checked the schematic multiple times for accuracy according to the datasheet. I've checked that the fab populated the correct components. The only load on this supply on power-up is the LED shown. The original chip on board wasn't working, so I replaced it with a new one. Immediately upon power-up, the LMR64010 burns out. The burn is by Pin 5, the 12V input.
The diode still measures good. Resistor values measure correct. LED is still operational. Capacitor values measure correct.
Here is my schematic:

Here is the layout:

Any ideas on what I'm doing wrong?
Thanks,
Mike