This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2121: Recommend device for battery pack protection

Part Number: TPS2121

hi Team,

OEMs wants to project the voltage input to the battery pack.

the abs max voltage for the pack+ pin is 30V,  they concern that externally might have 48V from the adaptor if the front end malfunction

the maximum current that can go in to the battery pack is ~12A. 

can you please help recommend a suitable device to prevent over-voltage event?

appreciate the help