Part Number: UCC28180
Other Parts Discussed in Thread: UCC256402
Hi
we are using ucc28180 as pfc controller for LLC converter 200W(28V,7A)
input :115Vac(85-125V),frequency=400Hz
we have first used input frequency of 50Hz.Converter is working fine.Now we increased the frequency to 400Hz. it is working fine but at higher loads we have oscillations at pfc output voltage.So we changed the compensation values. But ic is getting damaged on turn on. Gate pin is getting short to ground(20-100 ohms between gate and ground).
At 50Hz vcomp values are Cvcomp=5uF,Rvcomp=22.4k,Cparallel=0.5uF.
At 400Hz Cvcomp=2.2uF,Rvcomp=100k,Cparallel=0.1uF,
another iteration Cvcomp=1uF,Rvcomp=224k,Cparallel=5.6nF.
Gate resistor turn on 10ohms, turn off 5ohms. Gate pulses are clean and no spikes are present. Please help how to remove these oscillations.
Channel 1 : LLC Output Voltage
Channel 2 : PFC Output Voltage at 7A(input 85V)
Excel sheet attached.UCC28180 Design Calculator@400Hz.xls