Other Parts Discussed in Thread: BQ25606, BQ24079
Hi,
We have been using BQ24075/BQ25606 to charge the li-ion batteries. Because our system is mainly powered by mains, and li-ion is only used as backup when mains is off, so most of time li-ion batteries is idling at full charge. Over years, the battery will slowly and gradually degrade, eventually to the point that they can no longer provide any meaningful duration of back up.
I have learned that if we don't let li-ion batteries idle at full charge, but instead at 70 ~ 80%, their life will be greatly extended. BQ24075/BQ25606 etc. all come with a charge enable pin. So in theory, we can use external signals, such as GPIO pins from MCU to stop charging before battery reaches full charge.
Does TI have an application guild on how to go about this?
Update: after going through similar posts, I realized some charging IC terminates charging at 4.1V, such as BQ24079. I assume terminating at 4.1V will solve the problem.
So a related question is: is there any charging management IC that terminates at 4.1V? Particularly those with boost capabilities such as BQ25606?
Thanks in advance,
ZL