Initial Situation:
- We use the Texas Instruments-IC: BQ2000T
- We load a accumulator and when the threshold VMCV = 2.0V is reached at the BAT-Pin (PIN 4) the voltage-regulation starts
- And the accu will load full
=> So long is all OK
No the Problem:
- The Accumulator is a built in accu
- The accu is full and he has a self discharging (a few days)
- The voltage at the BAT-PIN drops from VMCV = 2,0V down
- When the threshold VRCH = 1,9V is reached (at the BAT-PIN), the IC should start a new charge-cycle
- And this new charge cycle do not happens
Questions:
- What is the problem, that don´t happen a new charge cycle ?
Best regards,
Markus