This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: Max pin current (RGE package)

Part Number: TPS1663

Hi, I was wondering if you can specific the max pin current for TPS16630RGER? Please note I'm not referring to the current limit threshold of the device, but the maximum current for a given input or output pin.

This is relevant in case one input or output pins is left floating, and the full current is channeled through a single pin instead of two. Thanks for your time!

Best regards,

Tristan