This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5067: Replace Rin with current source

Part Number: LM5067

Hi team,

When customer use LM5067, VEE vary from -15V to -50V. But the value of Rin require 2mA to VCC, which will cause large power consumption when VEE changed. So customer plan to use MOSFET to design a current source to supply 2mA to VCC. Is that ok? Any risk?

Another question is that in datasheet, there is 13V Vz which refer to the difference between VEE and VCC. But customer designed as typical application and tested VCC and VEE, they found that the VCC-VEE is only 9V. Could you pls analyze the reason? Thanks!

Rayna