This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3307: SENSE3 exceeding VDD+0.3V

Part Number: TPS3307


Hi team,

My customer wants to know if the device will get damaged when >VDD+0.3V is applied to SENSE3. From the related thread, I understood that SENSE3 should not exceed VDD+0.3V, which is shown in the recommended operating range. But since the AMR for SENSE3 is 7V, my customer wants to know if applying VDD+0.3V<VSENSE3<7V will lead the device to damage itself.

Could you kindly answer to this?

Regrads,

Ohashi