The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54319: Burnout issue of chips

Part Number: TPS54319

When we use TI's DC-DC TPS54319, we often experience inexplicable burning out of this IC during use, manifested as: the input/output PIN of TPS54319 is short circuited to ground, and the root cause has not been found;

Can you help find TI's engineers to provide a troubleshooting solution? We speculate that it may be parasitic inductance causing input voltage oscillation that exceeds the DC-DC withstand voltage value and causes damage, but we cannot verify it. Please also help confirm with TI's engineers if they have any experience or verification/simulation methods in this area. Thank you!

Usage scenario: This EVB is used for the module test board, and TPS54319 supplies power to the module (3.7V) on the EVB, with an input power of 5V adapter. During daily use, TPS54319 occasionally burns out, which occurs quite frequently. Sometimes, when used well, the IC burns out after re powering on, mostly during the EVB power-on stage.

From the monomer analysis of TPS54319, it can be seen that the input/output of the IC is both short circuited to ground. After replacing the IC, it can be used normally;

Please be aware of the above. If there is anything you need to provide, feel free to discuss it at any time. Thank you!

Core demands:Please help me analyze where there are problems and provide suggestions for modifications

The schematic and layout are as follows:

PCIE-CARD-EVB_SCH_V2.3_20200316.pdf

  • Hi,

    These kind of damages usually occur with input voltages above the ABS max ratings of the device. The customer could try out the following

    • Add a scope probe to the closest input cap C111 and set the scope to trigger for voltages > 6V. Run the board for a longer period of time to try and capture an input voltage spike
    • The customer mentioned the damage occurs more often during restart. To reduce the inrush current, the soft start time can be extended by increasing the SS cap value. Reducing the 220uF output cap can also help reduce the inrush currents. Can the customer share a scope shot of input voltage, output voltage and inductor current if possible?
    • Can the customer also try some long term tests without the 4 diodes D108 to D111? The diodes may also end up extending the time duration of spikes.
    • Can the layout file be shared?

    Best regards,

    Varun