Other Parts Discussed in Thread: BQSTUDIO
Hi,
I am using the I2C interface at 100kHz, the board reports all values correctly when using the Battery management studio. The problem I have is that when I read the cell voltage values using custom code, cell 8 reports incorrect voltages. From the technical reference manual Table 4-1 , I am reading back the cell voltage directly from address 0x23. Cells 1-7 are read back using the same address values from the table and these report voltages perfectly.
Do I have to apply any calibration coefficients to the cell values read from these addresses or are the addresses reporting cell voltages directly? Can you let me know the difference between my approach and the Battery Studio approach?
Thanks in advance
Richard