Other Parts Discussed in Thread: UCC28C42
Hi experts,
My customer is designing a DC/DC module product based on LM5021. For some reason they must use this part though it is not fully meet the application condition. To make the device fit the application, they shorted VIN and VCC pin together and powering the two pins with an 10V regulated supply, which input is powered from a bias coil. I understand this configuration will disable VIN UVLO function. They implement VIN UVLO with external circuit. Is there any other risk for this kind of configuration? There is a NOTE in datasheet says "It is not recommended that the bias winding be connected to the VCC pin of the LM5021. Doing so can cause the device to operate incorrectly or not at all.". Customer worry about the reliability of this kind of application circuit so need us help them verify.
Thank you!
John