This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27427EVM: BQ27427EVM Software Related Issues

Part Number: BQ27427EVM
Other Parts Discussed in Thread: BQ27427

hi,

1. Use BQ STUDIO software (version number 1.3.121) to write the design capacity to the DM area. After re powering on, it was not saved. The default value for the battery meter is 1340mAh, and the written value for the battery is 3500mAh. When writing, the photo is shown in the following figure;

2. 2. Occasionally, there may be an increase in battery power, a decrease in voltage, and a current display indicating charging, but actually discharging, as shown in the following figure;

  • Hello Jeno,

    bq27427 stores the data memory parameters in RAM. These will be lost on reset and will need to be written again.

    Check your current paths in case there is actual flow of current. If there is no current, then calibrate offsets and current gain.