The datasheet for this device specifies output capacitance values from 20-68uF. Are these values nominal values? Or are they referring to the effective capacitance values? Since these are high dielectric constant ceramic capacitors, they have a large de-rating based on DC bias. We are specifying two 47uF capacitors, which, nominally, is outside of the 20-68uF range. But the effective capacitance with de-rating is within the range. Is this the correct way to specify these capacitors?