This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51050B: How can I increase the BAT(output) current?

Part Number: BQ51050B

The current I want is about 500mA,

so I adjust I(lim, or Term)

But The output is only less than 50mA~20mA...

What should I do?

Is there anythings I nees to adjust or consider?