Having large failure on current product in the manufacturing line and field. The application is in LIDAR. One instance shows a burnt make in the device on pin 12. Below is the schematics.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Having large failure on current product in the manufacturing line and field. The application is in LIDAR. One instance shows a burnt make in the device on pin 12. Below is the schematics.

Hi Aden
Currently the issue I saw is that:
For Vin=24V Vo=1.5V, the D is small, =0.063 (even smaller when Vin=30V). The ton=D*Ts, which is very small considering the fsw is very high. For 24V->5V, 2.1MHz, the ton is around 30ns. Which is larger than the ton_min specified in the datasheet (Table 7.6).
The HS will keep conduction during the ton_min time.
Can the fsw be changed? Can 400kHz be used here? But you will need to select a larger Lm inductor if use 400kHz , I think ~4.7uH will be ok.
Thank you.