HiTeam,
could you please recommend a direct replacement for RUM002N05?
Is CSD18541F5 the best option here?
BR,
Stefan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HiTeam,
could you please recommend a direct replacement for RUM002N05?
Is CSD18541F5 the best option here?
BR,
Stefan
Stefan,
Yes it is the best option we have as per the cross reference tool.
However it is far superior in performance, some of the comparisons are:
TI Smaller:- TI Silicon package 60V 1.2mm2, vs comp 50V plastic package 1.44mm2.
TI Lower resistance:- TI 65mOhm max vs comp 2200mOhm max
As such it is likely we will be higher price due to this superior performance but is the closest/best fit device we can offer.
Thanks
Chris...