The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2662: TPS26621 no output

Part Number: TPS2662

The eFuse circuit is connected to the 3.3V regulator (using a resistor in place of L2/L3). Initially, L3 was populated, but the eFuse output showed 0V. Even after disconnecting L3, the eFuse output remained at 0V. To resolve the issue, I modified the 3.3V regulator circuit by disconnecting power from the eFuse output using L3 DNL and connected L2 to feed U3 power from the input of the eFuse. After this change, the eFuse output started functioning correctly. The continuous load current is approx 50mA.I have tested the circuit with Rlim = 20K, but still no output voltage.

The behavior of the eFuse output is puzzling and inconsistent when L2 is connected compared to when it is disconnected, regardless of the presence of L3.

Any pointer what could be wrong?