Hi, I have a problem with my board with a BQ40Z80 on it. I am in the testing phase of the product and I and I'm trying to test the effect of a high current on my board. I attached a load of 1Ohm on PACK+ and I'm supplying the circuit with a power supply and a simulated battery pack (6x1k in series). since the load is 1 Ohm power supply voltage is mostly the same as the current trough the circuit.
When I enable DSG FET trough BQ studio, the gate turns on(30ms) / off(3000ms) in a cycle as if something was pulling it down when it goes high. When I refresh register in BQ studio, I see that DSG is LOW but that XDSG is LOW too.
Output of the BQ at DCHRG pin:
The problem happens when I'm over roughly 18V/18A WITH A LOAD. Below that or without load, the DSG pin act in normal operation.
Since the DCHRG pin of the BQ40Z80 is only connected to the gate of the Mosfet, I assume that there might be a config that is set wrong in my BQ programmation. Could you help me find what could be the problem?
Here is the schematic of the region of interest:
Thanks in advance,
Karl