This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS60500 - outputting 2.5V not 1.2V

Other Parts Discussed in Thread: TPS60500

Hi,

I am using TPS60500 (High-Efficiency Step-Down Charge Pump ) for regulating voltage from 3.3V to 1.2V.  This 1.2V is used to power the CORE of microcontroller. But i am getting 2.5V instead of 1.2V. (ultimately MPU might have failed because of this, but how i'm getting 1.2V is still uncertain ???). Please help me to resolve this issue.

For you information:

Vin-3.3V, Feed back resistor (R1 - 100k, R2 - 200k).

capacitors value are seleced as per instruction in datasheet.

Note: I've used one more module, in that second module also having same problem.

Thank You