This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Solar cell battery charger

Other Parts Discussed in Thread: BQ25883, BQ25798

Please suggest me appropriate IC part number to charge 2 cell 18650 Li-ion battery (2S X 2P) having 7.2 Volts/ 6.4 A by triple junction GaAs 2 solar cells in series having Voltage range from 2.92 Volts to 5.26 and current from  470mA to  510mA. I also want alternate charging using USB as well if possible. I am using BQ25883 for USB charging and LTC4121 step-down battery charger. Since my Solar cells voltage has changed from 11 volts to 5 volts I now need to replace it with boost charger.