This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90160A: TI Fusion digital power designer software

Part Number: UCD90160A
Other Parts Discussed in Thread: UCD90160

Hi,

I was using TI Fusion digital power designer software and the problem I am facing is the following:

1) When using the systems monitor tab the Vout for the rails is not showing an accurate reading. When I supply 0.1V on the analog input MON1 the GUI is showing a reading of 0.2V. When I supply 1V at the input the GUI shows a reading of 2V. Why is this happening ?

Best Regards,

Shah Misbahul Huda