This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21750: Gate driver power supply control power budget.

Part Number: UCC21750

Dear experts,

Is there any analytical method to determine the control power budget required for the gate driver power supply ? My power supply is capable of delivering 80mA at 20V. My peak current requirement is 4.5A, calculated based on the equation given in the datasheet of UCC21750 for the selected Rg. How to calculate the rms current taken from the power supply ? LTSpice simulation can help i know, but is there any analytical method available, pls help. (the purpose is, incase of paralleling of mosfet required, whether this power supply alone can meet the power demand)

Thanks and regards

Anoop kumar N