This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25121A: Operation without PWM possible?

Part Number: BQ25121A


Hi,

I wonder whether the BQ25121A and my circuit can be operated from the LDO output only. I want to avoid the extra parts for PWM since I have very little space on my PCB and loads of 10 mA max. However, I am not sure if I get the default 2.5 V even without having power to pull LSCRTL high. I do have a devboard (for the 25120), but hesitate to remove the inductance there. Maybe I can get an answer without ruining the board ;-)

Regards, Peter