This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25982: Schematic check request

Part Number: TPS25982


Hello Sir:

Please refer our load current profile as below figure.

Our input voltage is 16.8V and max continue current is around 4.5A. 

Please help to check our schematic.

If there has any setting cannot meet our load profile or any side effects please let us know.

Looking forward your feedback.

Thanks a lot.

  • Hi Statham,

    Looks fine overall.  Are you planning to enable device through resistor divider from VIN or through some external signal on EN pin? Also you can consider transient protection if short at output can happen or there is long cable from supply to eFuse VIN.

    Regards

    Kunal Goel