Part Number: LM3648
Other Parts Discussed in Thread: LM36010, LM2759
Hi Sir,
If the LM3648 is in thermal shutdown, even if the die temperature is lower than 150°C, the LM3648 is not available for operation until there is an I2C read of the Flags1 Register and doing a read action, the Flags1 register is cleared, right?
My customer wonders why LM3648 should be designed with such a protection mechanism?(I mean need an I2C read)
They hope when the die temperature has lower than 150°C condition, the LM3648 can recover to normal operation automatically.