Hello,
UCC28070A's programmable peak current limit function (PKLMT) uses a signal voltage at CSA/CSB pins. Therefore, an output current when the peak current limit occurs may differ depending on the input voltage since a peak current that runs through a CT (i.e. external MOSFET) is not the same. For example, a signal voltage at CSA/CSB pins is different between the input voltage of 180 and 220 V, causing a different PKLMT threshold between them.
Is there a way to minimize the difference? Ideally, I want to have the same PKLMT threshold for the output current in the input voltage range from 180 to 220 V.
Best regards,
Shinichi Yokota