Part Number: TPSM33615
Hello,
Requesting you to provide me the VIH and VIL value of TPSM33615FRDNR as it is not mentioned in datasheet.
Regards,
Nachiketh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPSM33615
Hello,
Requesting you to provide me the VIH and VIL value of TPSM33615FRDNR as it is not mentioned in datasheet.
Regards,
Nachiketh
Hello Nachiketh,
I see. Please refer to the datasheet EC-table.

In order to get a guaranteed enabling and disabling of operation, your external control signal should satisfy the following, namely to cover the worst case conditions.
VIH > VEN_RISE = 1.3V
VIL < VEN_RISE - VEN_HYS = 1.16 - 0.404 = 0.756V
Hope this clarifies.
Best Regards,
Youhao