Hello.
TPSM33625 was reviewed by WEBENCH. Do the "IC Tj" and "IC Pd" displayed in WEBENCH include inductor losses in the module? The data sheet temperature distribution (page 36) shows an IC surface temperature of 69°C. Even with WEBENCH under the same conditions, "IC Tj" was as low as 40.21°C and did not appear to contain it. I just don't see an entry for inductor losses anywhere.