Hi I'm working with this BMS based on bq4050 and I have problems with the State Of Charge. When I wake up the battery after sending it to Shutdown to reduce the discharge the Relative State of Charge has changed. Could be that the BMS needs a cycle of charge and discharge to recalculate it? Does the BMS disconnect the DSG FET if the SOC is so low or does it just check the cell voltage?
Thanks