Hello,
I simulated the TPS2H000BQPWPRQ1 switch on PSpice for TI according to the reference design in the TIDUD43A file. As a result of the simulation, I saw that the current was at 20mA level. However, I could not read the current value from the CS pin. Although the SEL pin is connected to 5V in the reference design, I saw that I could read a voltage value proportional to the current value from the CS pin when I pulled the SEL pin LOW. Is there any harm in pulling the SEL pin LOW to measure the current while using the first channel of the integrated circuit?
I also want to reduce the current to 10mA instead of 20mA. For this, I replaced the 2.4kR resistor connected to the CL pin with 27.5kR. The current value dropped to 10mA, but this time I started to read a voltage above 4V from the CS pin. Reading a voltage above 4V from the CS pin shows that the integrated circuit is sending an error signal. What do I need to do to set the current to 10mA without error?
You can see the circuit according to reference design on Sim1.png and Result1.png. There is no CS signal.
The CS signal is correct and current is 20mA on Sim2.png and Result2.png after I pulled SEL pin to low.
The current is 10mA but CS pin shows fault on Sim3.png and Result3.png after I changed CL resistor value to 27.kR from 2.4kR
Thank you for your help.
Sincerely,