Hi,
In the Typical half bridge application of LMG3422R030 I saw that the input to S1 and S2 have lot of differences. If I am not wrong, the only difference should be that when its high input to S1 input to S2 should be low. I am not sure if there is some other difference in the 2 inputs. However, when I look at the circuit implementation I see that the isolator used has different pins, also there is a MOSFET MGSF1N02LT1G, to name few differences.
Could you please tell me why are the two branches different.
Thank you for your help,
Neha Agarwal