Part Number: UC3525A
May I know what is the output A/B Peak current? I think the 0.5A is an average current.
BR, Gary

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The 500mA source and sink is actually the absolute maximum rating, which is not to be exceeded to prevent device damage.
Under normal operating conditions the device does not exceed a peak of 400mA per output.
Thanks,
Mujtaba