Other Parts Discussed in Thread: TPS61033
we have this dev kit.
Test 1.
The input voltage is 3V/2Amp
Output voltage is set to 5V.
Test 2.
The input voltage is 4V/2Amp
Output voltage is set to 5V.
we are running a bench test. as soon we increase the load which consumes 300mA, the voltage output drop below input voltage.
Mode is set to Ground.
Also according to TPS61033 datasheet the input voltage range is 1.8V to 5.5V then why dos the EVM stats its input range is 3.6V to 5.5V ?
any insight ?