Hi,
I am using BQ25798 Battery Charge controller in one of our design.
1)I have question whether this IC can be used without battery only for buck and boost operation by providing Input source. If this can be used what are the configurations to be changed.
2) We are facing one more issue in terms of functionality for one of the test case mentioned below.
when battery is fully discharged and cut off the controller went to brown out state and switched off abruptly. During this time we provided Solar input which is connected at VAC1, Solar voltage is 4.3V, during this time battery is not charging and no output voltage at system load. We provided 12V to VAC2 but the Charge is not switching to VAC2. Can anyone help me out to resolve this issue.
Thanks & Regards,
Murali.
.