This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6594EVM: Unable to update demo kit with new state machine or script

Part Number: TPS6594EVM

Hi All,

I am learning to generate SPMI signals using the TPS6594x. I am experiencing two issues:

(1)

In the process of pushing several configurations to learn, the kit connected with only one device showing up (instead of 2, like before)

** Before and Expected: TPS65940 (M) + TPS65941

** Actual: TPS6590 (M) ----- no secondary device.

(2)

Assuming the kit is in a bad state, I've tried to push a new configuration.

It always fails with "Unable to unlock EEPROM" twice.

---

Desired help

(A) Help to reset the state, so it becomes programmable again.

----

Considerations:

(i) Is it possible the EEPROM is permanently locked? How does that look like?

(ii) Why is there only one device showing up?

Thank you!

Bulmaro H