Hi support team,
There is something I would like to confirm because a product with the TPS54335ADRCR has a defect in the inspection process.
【Questions】
1. Do you set a switching frequency of 480kHz (TYP) for the shipping test?
2. How many volts is the VIN input voltage in the shipping test to check the Vout output voltage?
3. Please let me know whether the PH output pin and other input/output pins have internal protection diodes (+, - direction).
4. The faulty device has about 10Ω between PH output and GND.
In this case, will it be rejected in the shipping test?
【Situation】
1. Device:
・TPS54335ADRCR
2. Operating conditions:
・VIN = 18V, Rrt = 100kΩ setting, switching frequency ≒ 480kHz (TYP), VOUT = 3.3V setting
3. Trouble occurrence:
・In-house shipping inspection process_substrate failure
・N = 1 unit (4 similar defects occurred in the past, 5th)
4. Bug details:
・DC-DC converter: 2_PH output abnormal waveform observed. (intermittent oscillation)
・Vout voltage output does not rise to 3.3V, only 1.5V..
・An overcurrent occurs and it falls into the current limit mode.
・After determining that the DC-DC converter was defective and replacing the parts, the output of Vout = +3.3V was normalized.
Regards,
Dice-K